Part Number: SN74AHCT244
part number SN74AHCT244MDWREP
Question 3,4,5,6 refer to a qual doc I have but I can get it uploaded in here. perhaps contact me and I can get the qual doc to you.
1. Was a c-SAM performed
2. Was a DPA performed
3. During the RH testing for 1000 hours, was the device powered or unpowered?
4. was the part powered for the whole 1000s or an on/off profile setup?
5. For operating life static test, it looks like it is powered during this test section is that true
6. In the qual report sent , it likes like TI is qualifying AHCT244DW by similarity to ACT240DW. I was asked how AHCT244DW is qual by sim to ACT240DW . What is the justification that allows TI to qual by sim to ACT240DW