Part Number: TXB0108
Other Parts Discussed in Thread: SN74AXC4T245
Hello all,
I'm using a TXB0108 8-Bit Bidirectional Voltage-Level Translator for my design instead of a TXS0104 device, to support 1.1V via the former. I have two questions regarding this:
1. Is it okay to leave the pins (A5-A8 & B5-B8) empty?
2. If experimented, does the level shifter 1.1V?\
Sorry if these feel like basic questions, need clarity.
Thanks & Regards,
Saurabh