Other Parts Discussed in Thread: SN74F112, SN74F109
Hi guys,
Below is a new customer inquiry:
I want to split down frequencies in range from 2MHz to 150MHz / 170MHz (if possible ... to 450MHz). It does not matter to me whether this is a counter or a JK flip-flop ... or another type of split. It should be possible to bring up the input frequency in the range of a few MHz. Ok is also a firm split factor of for example 4:1 or
x: 1.
Do you have such a device? If possible the price should be 2 or 3Euro max ... 70Cent would be even better. What I found is the JK-FF SN74F109 or SN74F112. However, according to the datasheet it can do only 114MHz. Is this correct or can I use this JK-FF also to 150MHz or 170MHz?
Here, the data from Farnel:
|
FAIRCHILD SEMICONDUCTOR |
IC, LOGIC GATE, FLIP-FLOP Flip-Flop type: JK; time, Transmission delay:6ns; Frequency:150MHz; Output Current: 24mA; Trigger type: Positive Edge; Supply voltage range: 2V to 6V; Logic IC package: SOIC: |
...but according to the datasheet anyway only 114MHz!!!
Thankful for help!
Kind regards M-Dizzle