Part Number: CD54HC4046A
Other Parts Discussed in Thread: SN74LV4046A, CD4046B
Does TI provide a model for their HC4046 family of PLLs?
Thx,
Rob
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CD54HC4046A
Other Parts Discussed in Thread: SN74LV4046A, CD4046B
Does TI provide a model for their HC4046 family of PLLs?
Thx,
Rob
Hi Emrys,
Thanks for the reply. What do you mean prototype only? They shouldn't be used for new designs? I'm looking for a PLL that will work in the 400kHz range, with or w/o an integral VCO. Any suggestions?
Rob
Hey Rob,
What do you mean prototype only?
I mean to say that there's no simulation model, so you must build a prototype to test your designs.
I'm looking for a PLL that will work in the 400kHz range, with or w/o an integral VCO. Any suggestions?
The '4046 will work at 400 kHz. The one thing to note is that this is a logic device, so your input and output should be square waves. I'd look at the SN74LV4046A, as that's the most modern option.
t must have PFD with push-pull charge pump output.
The '4046 has at least 2 phase comparators (CD4046B has 2, CD74HC4046 and SN74LV4046A have 3).
Although I recommend using the 'LV4046, the datasheet for CD74HC4046 is much better and is a great resource for designing with the LV4046.
All of these devices have push-pull outputs, but none of them contain a charge pump.
What about the CD4046B? Is there a disadvantage using a PLL w/o a charge pump. The charge pump will charge up the LF to a voltage to control the VCO. What I want to do is pull on the PFD output to induce a phase shift on the VCO. With a charge pump I can inject current into the output of PLL.
I think you're talking about an RF (sine wave) PLL, and I'm talking about a digital logic PLL (4046). They're similar, but my primary expertise is with the latter.
The CD4046B is designed for 15V operation, but it works from 3V to 18V. If I were operating with 5V or lower logic, I'd choose the SN74LV4046A.
This device will use a LPF to basically turn the pulse-chain output of the phase comparator into a DC signal that controls the VCO. You could use an analog adder circuit to modify that, but it's not something I've seen done before.