This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC125A-Q1: For long distance of SPI

Part Number: SN74LVC125A-Q1


Hello team,

Is it possible to use the buffer such as SN74LVC125A-Q1 for the SPI communication with 3m cable between master and slave? 

Or, can you recommend any automotive devices for the 3m SPI transmission (2ch x 4wire SPI)?

 

Thanks,

Sam Lee

  • LVC is the logic family with the strongest outputs. However, 3 m might be too long for single-ended signals, and in any case, the total capacitance of the cable limits the achievable speed.

    It might be possible, but you have to check the signal quality with an oscilloscope.

    If the LVC buffer does not work, consider using differential signals like LVDS or RS-422.