Part Number: SN74ALVC244
こんにちは、私はSN74ALVC244データシートについて質問があります。 絶対評価を持つViとVoの注意書きとして書かれた以下の詳細を教えてください。 「(2)入力と出力の電流定格が観測された場合、入力負電圧と出力電圧の定格を超える可能性があります。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74ALVC244
こんにちは、私はSN74ALVC244データシートについて質問があります。 絶対評価を持つViとVoの注意書きとして書かれた以下の詳細を教えてください。 「(2)入力と出力の電流定格が観測された場合、入力負電圧と出力電圧の定格を超える可能性があります。
The device might be damaged if any single of the absolute maximum ratings is exceeded.
But the VI/VO limits are an exception: if your circuit limits the current to less than 50 mA, then you are allowed to apply a voltage below −0.5 V or above VCC + 0.5 V.
Hi Hyuga,
As Clemens stated the VI can go below -0.5 V and VO can go up to VCC+ 0.5V with less than 50mA current on the I/Os. However, absolute maximum ratings do not imply functional operation of the device at these or any other conditions beyond those listed under Recommended Operating Conditions.
If briefly operating outside the Recommended Operating Conditions but within the Absolute Maximum Ratings, the device may not sustain damage, but it may not be fully functional. Operating the device in this manner may affect device reliability, functionality, performance, and shorten the device lifetime.
Regards,
Sebastian