This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0304: output capability

Part Number: TXB0304
Other Parts Discussed in Thread: SN74LVC125A, SN74AUC125

Hi Expert,

Due to AMD SPI  interface only support 4inch of driver length,  so customer would to use TXB0304 to extend the output drive length for SPI interface. 

if the SPI signal speed is 66MHz/bps to 100MHz, odes TXB0304 could to use here? if yes how long the distance of output driver length could support?

the device spec as attached. please help to check it.

or any more suitable solution to recommendation if TXB0304 can not support.

FLASH datasheet.pdf

Regards,

Mark