Other Parts Discussed in Thread: TXB0108
I have a customer with the following question:
The TXB0108 port B (5V) is connected to AD7716 and AT24C16 and there are some 4.7K pullups on port B outputs.
Port A (3.3V) is connected to a FPGA.
According to the TXB0108 data sheet and application SCEA043, a strong pullup (< 50K ohms) on port B is not recommended.
The legacy design engineer claimed he had tried that in the lab with 4.7Kohms pullup on port B outputs and they worked and did not see VOL problems (see attached bmp).
According to data sheet and app note, it should not work. Do I miss anything……please help.
Thanks, Saeb