This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G04-EP: Single Event Test Report

Part Number: SN74LVC1G04-EP
Other Parts Discussed in Thread: SN54AC14-SP, SN54AC00-DIE, SN54AC00-SP, SN54AC02-SP, SN54AC02-DIE, SN54LVC646A-SP

Dear TI Team,

Is there any report/document that contains single event effects information for SN74LVC1G04-EP?

Thank you.

  • Hi Tolgahan,

    No, I'm afraid we don't have any radiation data for that device.

    There are only 6 devices in the logic portfolio that do have radiation information (out of thousands):

    SN54AC14-SP

    SN54AC00-SP, SN54AC00-DIE

    SN54AC02-SP, SN54AC02-DIE

    SN54LVC646A-SP

    The 'AC00 devices have both TID and SEL, with rated values of 100 krad and 86 MeV-cm^2/mg -- the others are rated to TID 50 krad only.

    Regards,

    Sebastian