Part Number: CD4081B
Other Parts Discussed in Thread: CD4018B, SN74LVC1G08, SN74AHC08
Hi guys.
In my project I used the CMOS AND Gate CD4081B IC.
As you can see in the image below I place two NPN BJT (BC817-40) ad the outputs of two AND gate of CD4081B.
With 1kOhm base resistors, the current flow from pin 10 to the Q3 base is (4.6-0.7)/1k=3.9mA
I attend that the current flow from pin 4 is major than the above current, because that current supply Q3 base and the U5C inputs.
The datasheet of CD4018B say "Output High (Source) Current IOH min" is -1mA(typ) @25°C when the VDD is 5V (that is my case).

The problem is: how many current (max) can I sourced from the two outputs (pin 4 and pin 10)? I think the CD4081B can't give the current that I need.
BR,
Gabriele.