Part Number: CD4541B
Other Parts Discussed in Thread: SN74LVC1G14, SN74HCT74, CD74HC4040, CD74HC163
I am contracting with a customer and need your help with their circuit that uses the CD4541B. The frequency we measure on the bench does not equate to the formula and configuration details in the data sheet. Rtc is 56K, Ctc is 0.5pF and RS is 113K. The device is configured to divide by 256. The frequency of the square wave being output from the CD4541B measures to be 6.41 kHz. However, using Rtc & Ctc to calculate f, then dividing by 256 gives a calculated output frequency of 60.7 kHz. Off by a factor of 10.