Hi TI Partners,
Could you help to make sure the Guaranteed max VOL VS IOL curve from Tamb 25℃~85℃,when SN74LVC07ADR with VCC 3.3V supply ,and when the IOL is between 0.5A~10mA.
From datasheet, I can only find the Guaranteed MAX VOL 0.55V@IOL 24mA ,but I can not find the curve .
BR
Cheney SUN