Part Number: TIC12400-Q1
Hi Team,
May I know the sampling is a specific value or a range for the analog input?
Frank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIC12400-Q1
Hi Team,
May I know the sampling is a specific value or a range for the analog input?
Frank
Hi Frank,
Each device input can be configured in comparator input mode or ADC input mode. When an input is configured as comparator input mode, the threshold level for interrupt generation can be programmed to one of four available threshold levels: 2.0V, 2.7V, 3.0V, and 4.0V. When an input is configured as ADC input mode, the threshold level for interrupt generation can be configured from 0 to 1023 different levels. See datasheet section 8.3.8.4 for more detailed information.
Let me know if you have any more questions.
Regards,
Eric Schott