Part Number: SN74AHC541
Other Parts Discussed in Thread: SN74HCS541
Hi Team,
Customer wants to verify this, max rating shows input cannot be over 7V max, however, in the note1, it seems to imply input voltage can be higher than 7V as long as input current less than 20mA, is it true?
Anything else needs to be aware of if customer must operating with input voltage over 7V? Thanks!
Andrew