Part Number: LSF0108
Other Parts Discussed in Thread: LSF0101, TINA-TI, PCA9306
Hi all,
I am using LSF0108 as a level shift between 1.8V to 3.3V and 3.3V to 1.8V, when doing the SI simulation, which series model should I use?


Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Tommy,
Select the model that corresponds with the planned VrefB voltage, so in your case 3.3 V.
Hi Dylan,
Sorry to sking another question
after simulating the level shift between 1.8V to 3.3V(please see the pictiure below)

Red line is output by using series model: LSF0101_IO_18_S
Green line is otput by using series model: LSF0101_IO_33_S
as the simulation result can see
it's shows using LSF0101_IO_18_S may can level shift 1.8V to 3.3V
it's different that you told me "Select the model that corresponds with the planned VrefB voltage, so in your case 3.3 V."
is there have any comment or reson you can tell me why?
thanks
Tommy
Hi Dylan,
sure,please the picture below

the simulation point is U8
the different is ones is use series model: LSF0101_IO_33_S and the other is series model: LSF0101_IO_18_S
the result is the picture i send it yesterday.
thanks
Tommy
Hi Dylan,
sorry to disturb you again
I'm afraid of some misunderstanding between us
I want to share my Hyperlynx file to you
do you guys have Hyperlynx lincense?
please help to setup LSF0108 properly for us
thanks
Tommy
Hey Tommy,
Thanks for added info. I'll pass this to our modeling expert to dig into, please give them 24 hours to ramp up on the issue and provide feedback.
Hi Tommy,
I am looking into this to see what is the issue. I am waiting on the hyperlynx license as I cannot open the file otherwise.
Are you able to use TINA-TI or PSPICE to simulate? We have working models in that case.
Regards,
Karan
Hi Karan
No, we don't have PSPICE to simulate it, but we do download the TINA-TI.

From 1581.LSF0108_Behavioral.cir, we can know what's the corresponding volt for each pin/model.
Looks to me like the series model connects to EN pin, and EN is the same as VREFB.
So, I think we should use 3.3V series model in simulation when we do level shift from1.8V to 3.3V.
But, the simulation results are not what we think.

Hi Klaus,
Thats correct, you should be using the 3.3V series model but something in the model is not working.
Yes the data may be different but the PCA9306 has a similar model architecture. Are you able to use the PCA9306 IBIS model?
Regards,
Karan
Hi Karan
Yes, from your schematic, we should use 3.3V, since EN connects to VEFB, but just like what you said, something in the model is not working.
We've compared LSF0108 and PCA9306 series model looks like both behaviors are the same, so I don't think PCA9306 will work.
Klaus
Hi Karan
For IBIS file, do you have any suggestions? or can we use another one?
Klaus
Hi Klaus,
Unfortunately I am not able to figure out why the IBIS model is not working. It looks like the data is there but it is giving opposite values.
I will suggest you try to use the TINA model as it is fairly accurate.
Regards,
Karan
Hi Karan
I think we still need to figure out why the series model is not working
Since we've verified HyperLynx tool and we also used many IBIS files in HyperLynx, such as i2c switch, level shifting, etc.
For those components I mentioned above, it always has the series model in the IBIS file.
Could you get the HyperLynx license? so that we can compare apple-to-apple.
Thanks
Klaus
Klaus,
I built the circuit myself and am getting the same results as you. If you use the fast-strong model, that works correctly. I believe the data collected in the model for the 3.3V node is very weak.
Also, the supply voltage only sets the bias voltage for the FETS however you can still translate at any voltage higher. So if you use the 1.8V model and connect externally to 3.3V supply then that is okay to do.
Regards,
Karan
Hi Karan
Regarding the fast-strong model, does it mean the strongly driven strength of the driver? like CPU.
Both read and write, is the same? I mean using the 1.8V series model for read and write.
Thanks
Klaus
Hey Klaus,
Today is a U.S. Holiday, please give Karan until Monday to reply. Until then, I recommend watching these training videos on LSF to understand how it functions. This may better help you to understand some of the things discussed.
Hi Dyan
Sure, I watched it before, but it's incorrect when using 3.3V series model in the simulation, so that's why we would like to confirm with Karan.
Looks like we could use 1.8V series model in the series model, but we're not sure is it ok for both read and write.
Thanks
Klaus
Hi Klaus,
Yes you can use the 1.8V series model for both read and write scenarios.
The fast-strong model is when the supply voltage varies to 3.6V, the temp drops to -40C and the silicon is in its strong corner build.
Regards,
Karan