We are using the SN74LVC14APW device, and have a few questions:
1) Any data that shows how the Vih min varies over temperature? If we interpolate 3.3V VCC over entire operating temperature range, we get about 1.0V, but don’t know if that number is higher or lower at high temps or low temps. Our operating temp range is only a subset of the part’s range (-40C to +75C), so we want to knw how this parameter varies between those endpoints.
2) Same thing as above, but for Vil max.
3) Also want to know min and max impedances to both GND and the VCC supply rail.
4) Also, the max slew rates allowed for both rising and falling edges (5% to 95%) over the temperature range mentioned above.
If you have this info as in a curve format, good, otherwise the worst case over the entire operating range of the device will do.
We need this info urgently, any help will be greatly appreciated.
regards