Part Number: SN74LVC1G00
Typically pullup resistor values for logic inputs are in the range of 4.7K ohm to 10K ohm.
However, there are some situations where I would like to use a higher value.
This is usually to save power, or when the driving device does not have high enough sinking current ability.
Can you please recommend a MAXIMUM pullup resistor value that can be used with LVC inputs?
i.e. can 100K ohm be used?
NOTE: If there are different constraints due to DC input characteristics as compared to input rise time, please differentiate these in your response.