This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74ACT14: IBIS Model questions

Part Number: SN74ACT14


Hi team,

1) Is SN74ACT14 IBIS Model generated from SN74ACT14 Behavioral SPICE Model?

2)This says SN74ACT14 Behavioral SPICE Model has errors, SN74ACT14 IBIS Model so?

        e2e.ti.com/.../4076091

Best Regards, tak

  • 1) Is SN74ACT14 IBIS Model generated from SN74ACT14 Behavioral SPICE Model?

    No. IBIS models are built from either internal simulations (hspice or spectre) or actual performance of the device (physical silicon). They are much more accurate than the behavioral models which are only intended to provide a general understanding of operation.

    2)This says SN74ACT14 Behavioral SPICE Model has errors, SN74ACT14 IBIS Model so?

    Yes, that is correct. The fix described there is still valid.

  • Thanks.

    2)This says SN74ACT14 Behavioral SPICE Model has errors, SN74ACT14 IBIS Model so?

    Yes, that is correct. The fix described there is still valid.

    When will the modified SN74ACT14 IBIS Model be uploaded?

  • The IBIS model is not going to be modified. As I said previously, these are separately created models. The Behavioral SPICE model does not have any impact on the IBIS model.