Other Parts Discussed in Thread: TXU0304, TXU0104, TXU0204
I find that the outputs gets latched and does not recover if loaded by a capacitive load, eg. A digital multimeter. In the datasheet is says there is a "one shot" pulse generated to improve the IO slew, but based on my experiment, it seems like it is level triggered and it can last forever, so it is not one shot. I have low voltage input toggling at 5Hz rate and try to measure the level with multimeter on the high voltage side. The high voltage side gets stuck at 1.6V and input is around .8V and it sinks/sources current such that 2mA driver cannot drive it between 0 and 1.8V,
Atul