This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LS06: The same device for SN74LS06DBR.

Guru 11285 points
Part Number: SN74LS06
Other Parts Discussed in Thread: SN74AHC05, SN74LV06A

Hi team,

My customer is having trouble because they can't get SN74LS06DBR.
Do you have a similar device with the same PKG?
It is difficult for them to change the design because it is in mass production.

Sincerely.
Kengo.

  • Hi Kengo,

    It will depend on how they are using the device. What are the applied voltages? Signals? Loading?

    The 'LS06 is fairly unique in the logic portfolio, as it is the only device I know of that supports a 5V supply and 30V output voltage, so there may be no option for replacement.

  • There is no compatible device with high-current, high-voltage outputs.

    If you do not actually need the high voltage, you could try the SN74LV06A or SN74AHC05 with less drive strength (they are out of stock at TI, but Mouser still has some).