SN74LV126APWR:最大定格-0.5Vを超えるアンダーシュート波形を測定しました。
ICの許容電圧を教えていただけますか?
また、-0.5Vを超える条件の許容期間についても教えてください。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SN74LV126APWR:最大定格-0.5Vを超えるアンダーシュート波形を測定しました。
ICの許容電圧を教えていただけますか?
また、-0.5Vを超える条件の許容期間についても教えてください。
Thank you for your reply. And I'm sorry.
Measured undershoot waveforms above the maximum rating of -0.5V. Can you tell me the allowable voltage of the IC? Also, please tell me about the allowable period for conditions exceeding -0.5V.
Hello Kishimoto-san,
There is no allowable period for exceeding -0.5V. This value can be exceeded so long as the current through the clamp diode is limited to the value provided in the datasheet. This information is in the absolute maximum ratings table here:

Thank you for your reply.
Other than the current,It exceeds about 3ns (-0.5V), but I would like to confirm if it is within the allowable range.
As a guide, how many ns is the allowable period?
There is no alloweable period for a higher current.
But, according to the IBIS model, a current of −20 mA requires a voltage of at least −0.74 V in the worst case. What is the peak voltage?
The positive limit is 7 V.
Thank you for your reply.
Peak voltage is -0.69V.
The period from -0.5V to -0.69V and -0.69V to -0.5V is 3ns.