Part Number: TXB0108
Other Parts Discussed in Thread: TXS0108E, , SN74LS640
Hi
If the input of port A becomes high active and the input of B port becomes low active at the same time, is there any problem?
Also, when inserting pull-up resistors on both sides, 50kΩ is used, and is there anything else to be aware of other than the drive strength ± 2mA?