This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Input tolerant single gate logic for 10G signals



Hi Experts,

Would you kindly help with this inquiry?

the customer is trying to voltage level shift down 10G data signals from 1.8V to 1.2V.  they read an application note describing level shifting using single supply one-gate logic (like an AND or OR gate) that is input tolerant.  can you help suggest an input tolerant single gate logic, or something else, to help level shift down at 10G.

Thanks in advance.

Regards,

Marvin