This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVCC4245A: A1-8 pin behavior, when VCCB=0V and B1-8 is supplied to 3.3V.

Part Number: SN74LVCC4245A

Hi,

Under the following SN74LVCC4245A's condition,

  • VCCA : 5V
  • A1-8 pin : Output
  • B1-8 pin : Input

When VCCB=0V and B1-8 is supplied to 3.3V, what is occurred on A1-8 pin?

  • A1-8 may be damaged.
  • A1-8 = 0V
  • A1-8 = 5V
  • A1-8 is unknown state
  •                                       etc.

Please advise us.   My customer is making FMEA.

Thanks and best regards,
M.HATTORI.