This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G175: SN74LVC1G175

Part Number: SN74LVC1G175


Hi,

Can you recommend a Schmitt-trigger input single D-type rising-edge-triggered flip-flop. 

Basically he wants to drive with one fast drive edge and that is all, He wants to avoid using the external Schmitt-triggers shown in the configuration below.

Thanks

Jani

  • Hi Jani,

    We have no single input D-Type Flip Flops with Schmitt-Trigger inputs.

    We have a 2 channel D-Type Flip Flop with slightly different functionality: SN74HCS74. This device is offered in the DYY package which is our smallest 14-pin package available.

    Note the HCS family supports a supply voltage of (2-V to 6-V) and has lower drive strength (7.8mA at 6V Vcc) compared to LVC. 

    Regards,

    Sebastian