This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVCH16T245: SN74LVCH16T245 max peak output current

Part Number: SN74LVCH16T245


HI,

One of my customer is asking about our SN74LVCH16T245

 

They are using a 5V output, that will drive a RC circuit (100kHz, 3.3nF) at 110kHz

 

Could you please comment on the device max output peak current?

The datasheet mentions +-50mA, but the figures shows VOH/VOL value for current up to +-100mA, so I wanted to run it by you and get your feedback on this

Thanks for your help

Foucauld