This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4072B: Sinking current at 3.3V

Part Number: CD4072B

Our design choose CD4072B working at 3.3V supply. So I need to know about the sinking current at 3.3V, since the device's datasheet doesn't appeared parameter for 3.3V. Thank you in advance.
  • CD4000 devices are designed for higher voltages. At 3.3 V, there are no guaranteed electrical characteristics. The sinking current is likely to be much worse than that at 5 V, probably no more than 20 µA.

    You should use OR gates from a family like LVC. If you need four inputs, combine multiple OR gates.