Other Parts Discussed in Thread: TXU0304
Hi, TI Support Team
Inquiries regarding the following items have been received from customers.
TXS0108EPWR product is being used and SPI and data signal are input as input.
The clock is 18.8 MHz.
Vcca=3.3V
Vvvb=5V
The output waveform is distorted and output, please review what is the cause.
Below is the circuit diagram. Please review the circuit diagram for errors.

There is a possibility that it may be affected by the clock, so I changed it to TXB0108PW and tested it, but the waveform is distorted in the same way.
Thanks.
Regards,
MJ