Other Parts Discussed in Thread: SN74LV14A
Hi Team,
Since following thread is locked, let me open a new thread.
Since datasheet said "device can exceed -0.5V as long as IIK is lower than 50mA(SN74VMEH22501A) and 20mA(SN74LV14A) respectively", and Clemens said IIK can be estimated from IBIS model. Customer have 2 questions as following.
1. Customer confirmed VMEH22501A_IO_3B pin, but it comes out I(min) is larger than I(max) when V=-0.665V, is it normal?


2. Vpeak of undershoot = -0.54V in customer application, I is -30mA for worst case when VIN=-0.6V, so does it mean it is NG since exceeding abs. max rating which is 20mA?

Thanks.
Regards,
Jo