Part Number: SN74LV123A
Hello,
I'm trying to simulate a falling edge detection using the SN74LV123A. The input signal (/A) is high @t0. Then it changes to low and remains low for 1us only. When the falling edge is detected the output (/Q) should change to low and should remain low for 230ms approximately. To do so i used Rext = 490k & Cext = 470nF.
The problem is that when I run the simulation the output /Q does not change as you can see below :

Green = /A
Blue = /Q
Red = Rext_Cext
Thank you in advance for your assistance.
Sincerely,
Achraf