Hi team E2E!
I am working with the LED Matrix Manager (TPS92664-Q1), actually i made the comunnication, but I'am having problems to get the frames to start the sequence of the leds, i´m not sure if i need a previous configuration or something else. i am reading the datasheet of the divice, and in the page 78 there is the Figure 9-4. TPS92664-Q1 Initialization Logic Diagram, do i need to follow all the steps on this diagram to turn on the leds? another doubt, in certain part i try to write in the register MTPCFG (0x00) but when i read that register i dont have the bits that i wrote, do you have any recomendation to start my sequence? I have read that i need to write into the widthx, phasex, and ledon registers to turn on the leds, thats right? do you have any example to turn on the leds or any sequence for that?
thanks for your support