Dear Specialists,
My customer is considering TXS02612 and has a question.
I would be grateful if you could advise.
---
We have a question about TXS02612RTW.
We are currently developing products (COM Express board, COM Express carrier board) that implement TXS02612RTW.
TXS02612RTW is used for voltage level conversion between CPU (1.8V series) and SD Card socket (3.3V series), and is mounted on the COM Express board side.
(Could you please see the block diagram in the attachment).
When I inserted the SD Card into the SD Card socket and checked the operation, the CPU did not recognize the SD Card, so I debugged and measured the waveform.
As a result, it was found that the CMD waveform was distorted and reflected noise was generated when the clock frequency was operating at 50 MHz.
(Could you please see the waveform in the attachment).
When the clock frequency was lowered to about 1MHz, the CPU recognized the SD Card and confirmed that the waveform was not distorted.
Could you please let us know about the possible reasons for these and how to fix with them (such as the placement position of parts and the regulation of wiring length)?
As reference information, the wiring length is as follows.
CPU <-> TXS02612RTW: About 20mm
TXS02612RTW <-> COMe Connector wiring length: about 100 mm
COMe Connector <-> SD Card socket wiring length: about 150mm
---
I appreciate your great help in advance.
Best regards,
Shinichi