Other Parts Discussed in Thread: SN74LXC8T245, SN74LXC2T45, SN74LXC1T45, SN74LVC16T245, SN74LV125A, SN74LV4051A, TMUX1208, SN74LVC1G125, TXB0104, SN74LV125, TXB0108
Hi,
We are looking for bidirectional buffer/level translator for one of our application. We have 48 gpios which can act as both input and output(configurable in SW). We want to increase drive strength(upto 5mA) of microcontroller by adding buffer . Microcontroller operates at 5V level and hence we are looking for bi-directional buffer with 5V translation in either direction as any gpio can act as input or output. We have gone through multiple level translators chips which states for translation at VCCA(low side)<=VCCB(high side) for upto 5.5V but they also mention for proper operation, VCCA should be lesser than VCCB. So we are little confused if chip can be used by supplying 5V on either end or not. Can anyone please suggest any chip which can serve our purpose.
Regards
Narendra Singh