Other Parts Discussed in Thread: SN74HCS151
Hello Team,
Could you please help with the following question regarding the use case of SN74AXC4T774 as level translator together with 2 SPI slaves as described in the app note SCEA065B figure 2-2?
The issue is on MISO side because it appears that when SPI slave MISO has its output Hi-Z, the output of the SN74AXC4T774RSVR A3 (U4001) is not set Hi-Z but Low level. So when the second SPI A4 pin (U8501) slave send a High level, the signal is short-circuited to the low level between both level translator A3 (U4001) and A4 pin (U8501).
So we think that the suggested architecture in figure 2-2 might not work.
Maybe 2 solutions:
- Solution 1: Connect the #OE signal to SPI Slave Chip Select -> in this case when the device is not selected MISO output (in level translator point of view) is Hi-Z
- Solution 2: group together all MISO signal from Slave (as they have the same potential) and connect them to a unique input of a level translator -> In this case the Hi-Z state and short between MISO will not appear
What do you suggest? Do you have an alternate solution?
Regards,
Viktor