On my project, we need to translate between 1.8V (input) and 3.3V (output) using the SN74AVCB164245, and i need to make sure the output rise/fall time meets our requirements. However, i have been having issues finding this. There is no reference to output rise/fall time in the datasheet, only input.
I was given this forum showing how to calculate the rise/fall time given the Voh, Vol, Ioh, and Iol: (+) [FAQ] What is the output transition rate for a logic device? - Logic forum - Logic - TI E2E support forums
However, i do not know exactly which values to use to calculate it. When i tried to calculate it, i got that the Roh and Rol were exactly the same (16.67 ohms), but the attached forum seems to show that there are two different resistance values (though they were pretty close).
Also, i am not sure exactly what capacitance i should use. The forum seemed to use an arbitrary 50 pF load capacitance.
Some clarification on this would be greatly appreciated.
Thanks.
Screenshots of the electrical characteristics & recommended operating conditions for reference: