Part Number: SN74LV125A
Other Parts Discussed in Thread: SN74LVC125A, SN74AUC125
We are using the buffer SN74LV125ADGV. The input, given to the buffer, is a 48MHz oscillator frequency and the output is connected to 4 MCUs, as external clock input, through 4 output channels of the buffer.
We would like your opinion on this approach if it would work or not and please do suggest the best feasible option for the same.