Other Parts Discussed in Thread: TXU0101
Hi
First I apologies for asking so many questions regarding SPI logic Translator since I never deal with SPI logic translator.
I have two different SPI salves and I decided to use two of TXU0304. I have two questions:
1. Since TXU0304 have internal pull down, do I still have to pull up, or down chip select of each SPI slaves
2. Since I have Two chip select I have to use two TX0304 which method is correct way to wire it:
Option #1: As you can see in this option I am using second TXU0304 just for chip select 2. I prefer this way since I have to add single terminating resistor per output.

Option#2: Instead of sharing the low voltage output, we share input.

Is there better way to do this?
Please let me know if you have any questions
Thanks again
Please let me know if you have any questions.
Thanks