Regarding the TXB0104Q Bi-directional Translator: What is the maximum IOH and IOL for a 5V output? The data sheet seems to indicate it is 20UA. Is this the correct number to use?
Thank you ,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Regarding the TXB0104Q Bi-directional Translator: What is the maximum IOH and IOL for a 5V output? The data sheet seems to indicate it is 20UA. Is this the correct number to use?
Thank you ,
Are there any parts in the TXU series in the 12-UFQN package that are bi-directional? The circuit board is already done, and I am seeing signs that the line is overloaded.
The datasheet recommends using pullup/pulldowns that are 50K or greater in value. If the max IOH was 20uA, this signal would never be driven to the appropriate levels? Could you please recheck to make sure the max drive is actually 20uA? Thanks.
The TXU is not bidirectional.
It is not possible to buffer fast bidirectional signals. The TXB cannot be used with long traces, connectors, or cables.
The 50 kΩ limit ensures that the resistor is weaker than the TXB output. (If the resistor were stronger, the output would not work at all.)
I will place a 74LV1G125 in series with the output to give it more drive. Thank you very much for your help.
The '125 is not bidirectional. If you have a direction control signal, use a direction-controlled translator like the SN74AXC8T245.