This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVTH16244A: Alternate part number without bus hold

Part Number: SN74LVTH16244A
Other Parts Discussed in Thread: SN74AHC16244, SN74LVC16244A

Hi,

I was searching for alternate part for SN74LVTH16244ADL without bus hold circuit. Im looking for 16 bit buffer with 5V tolerant input with VCC 3.3V . I want to preset output value for few signals and PULL up resistors are not recommended for bus hold circuit.

Thanks