Part Number: TXB0104
Other Parts Discussed in Thread: TXU0304
Using TXB0104 to translate SPI from master 1.8V PHY to slave 3.3V Flash. Turns out that the PHY PU does not have enough drive strength on one SPI bus lines for proper operation. Placing a 1K PU on the 1.8V line starts working, while the other bus lines work without additional pull-ups. Other than the decreased VOH and VOL from the PU, are there any other concerns with such low pull-ups tied to the translator?