This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0102: VoltageB-Side (Vref_B) range

Part Number: LSF0102

There is confirmation in the LSF0102 datasheet.
<DataSheet Rev.K>
www.ti.com/.../LSF0102


There are two ways to describe Vref_B.
-------------
1: 6.3 Recommended Operating Condition (Page5)
  Vref_B max5.0V

2: Table 9-2. Application Operating Condition
  Vref_B max5.5V
-------------

Can you use Vref_B and Vpu(B) between 5V and 5.5V?
We think that there is no problem if it is the description method of No.2.