This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AND gate for Laser System



Hi Team, seeking for some inputs.

In need of an AND logic gate for a project. Need to generate a trigger signal for our laser system or in need to use a TTL burst to select TTL pulses from a pulse train. One of the lasers is triggered with a continuous TTL pulse train. The laser produces a laser pulse for each of TTL pulses in the train. However, we do not want the laser to produce a continuous laser pulses. Thus we would like to modify the trigger signal for the laser. We would like to use device (like a AND gate or a relay, or other device) to modify the trigger pulse train.

I will use a computer to generate a TTL pulse burst, which will be used to modify the pulse train. The TTL pulse train and The TTL burst have the same repetition rate. I plan to use the computer-generated TTL pulse burst to slice/chop/select pulses from the TTL pulse train.

The pulse duration of the TTL pulse train is from 50 micro-second to a few millisecond. The pulse duration of the burst can be any value.

 

Do we have any solution for this specific application?

Thank you.

-Mark