This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AXC2T245-Q1: 1.8V I/O model not found in IBIS model

Part Number: SN74AXC2T245-Q1
Other Parts Discussed in Thread: SN74AXC2T245

Hi,

We are using CAXC2T245QRSWRQ1 in our design for level shifting of voltage from +3.3V to +1.8V. We need to perform SI analysis. 

The models found in sn74axc2t245.ibs are io_0p7 and io_3p3. And no 1.8V I/O model is available. 

Our query is there any other IBIS model having +1.8V I/O model that we can use as an alternative for sn74axc2t245.ibs?

Can we use the IBIS model in the following link: SN74AXC2T45 data sheet, product information and support | TI.com as an alternative?