Part Number: SN74LVC16245A
Hi team,
This request is for all TI products. I described the part number because it's required filed.
This request is related to environment, so we've requested this to CSC with case No.CS1185134 first of all.
However we couldn't get enough information from CSC. Please see the case No if you need to see.
*** Request ***
Could you make sure if the following substances are included in inks used for TI products and packaging materials for shipping the products above the threshold level ?
Since we've got same request from some major customers, this request will increase. We hope that TI issues company letter and post in ti.com so that customers can make sure soon.
[ Outline of legal requirements ]
(1) Name of the regulation
Order of April 13, 2022, specifying the substances contained in mineral oils prohibited for use on packaging and for printed matter distributed to the public.
https://www.legifrance.gouv.fr/jorf/id/JORFTEXT000045733481
(2) Subject to regulation
- Specific mineral oils contained in the printing ink of packaging materials
- Specific mineral oils contained in the ink of printed matters
- Definition of mineral oil: oils produced from feedstocks derived from petroleum hydrocarbons used in the manufacture of inks
(3) Banned substances and prohibitions
- Mineral oil aromatic hydrocarbons consisting of 1 to 7 aromatic cycles (MOAH)
Effective from Jan. 1, 2023 : The concentration in ink exceeds 1%
Effective from Jan. 1, 2025 : The concentration in ink exceeds 0.1%. The concentration in the ink of compounds with 3 to 7 aromatic cycles exceeds 1 ppm.
- Mineral oil saturated hydrocarbons consisting of 16 to 35 carbon atoms(MOSH)
Effective from Jan. 1, 2025 : The mass concentration in ink exceeds 0.1%
Thanks,