I've observed that the SN74LVC1G34 output strongly tracks its VCC during power-on, until VCC crosses its power-on threshold. It takes quite a small pull-down resistance to prevent this power-on "glitch". Is this expected behavior? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I've observed that the SN74LVC1G34 output strongly tracks its VCC during power-on, until VCC crosses its power-on threshold. It takes quite a small pull-down resistance to prevent this power-on "glitch". Is this expected behavior? Thanks.
This can be normal. When Vcc is at 0V the I/O's are high impedance so they may float then. during the power up the output may rise with vcc until the part turns on at about 1V for LVC.
To be clear, the output is not just floating up as VCC rises. It is sourcing current, and it takes a lot of current to pull it down. Is it normal behavior for the output to be driving strongly (not high impedance) during power-on?
Are you suggesting that the output can actually interpret the input as VCC ramps up from 0V (before 1.5V)?
LVC normall turns on about 1.2V however the LVC little logic is newer process that may turn on lower. some of out other little logic parts begin to work at .5V.
I have no data either way but its worth a try.