This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] SN74HCS595-Q1: How do Wettable Flank WQFN packages (WBQB) help LOGIC automotive customers?

Part Number: SN74HCS595-Q1
Other Parts Discussed in Thread: SN74HCS138-Q1, SN74HCS151-Q1, SN74HCS153-Q1, SN74HCS157-Q1, SN74HCS165-Q1, SN74HCS259-Q1, SN74HCS365-Q1, SN74HCS367-Q1, SN74HCS594-Q1,

Efficient Automated Optical Inspection (AOI) with new TI LOGIC Wettable Flank devices

               Looking at the automotive market today, there continues to be growing trend towards smaller PCBs for a wide variety of applications. Though it has become apparent more recently, the simple fact is that board space comes at a premium, which has driven demand for non-leaded package options for many popular LOGIC functions such as shift registers, gates, and buffers.

               This seems like a valid solution as non-leaded packages typically have smaller footprints, but it creates a problem for automotive customers attempting to qualify these parts. Due to the nature of the solder between the board and the QFN package, it is difficult for standard camera-based AOI (Automated Optical Inspection) to fully “see” the quality of the soldered connection and qualify the part. Instead, advanced, expensive, and difficult to maintain X-ray technology must be utilized in order get a visual on the solder quality, which is not optimal and sometimes not an option for automotive customers.

         

Figure 1: Commonly Used WQFN Non-Leaded package and pinout for 595 (shift register) function

 

        

Figure 2: Dual footprint visuals, comparing PW (TSSOP-14 pin) and BQA (WQFN-14 pin) packages. The non-leaded BQA (WQFN) package takes up approximately 30% less board space

               

The solution to the issue of qualifying non-leaded packages is the wettable flank modification. A wettable flank is typically a dimpled or step cut package modification, which creates an opportunity for the solder to readily form side fillets after soldering. This allows AOI to better view the soldered connection, and qualify the part in an efficient and cost-effective manner.  

Package view

BQB0016A (standard WQFN pkg) - BQB

BQB0016B (WQFN pkg with WF modification) - WBQB

Top View

Side View

Figure 3: Side by side WQFN packages, highlighting wettable flank dimple cut modification (595 function)

Figure 4: Visual of how Wettable flanks allow for optimal AOI inspection for nonleaded packages

               Here are some examples of the new LOGIC AEC-Q100 qualified devices that have the wettable flank package modification, ensuring efficient inspection by AOI. The “BQB” in the orderable part number is indicative of the WQFN (Very Very Thin Quad Flat No Lead) package, while the “W” represents the device having the wettable flank modification/capability. Feel free to click on the WF OPNs below for more information and datasheets.

Generic part number (GPN)

Orderable part number (OPN)

Function

SN74HCS138-Q1

SN74HCS138QWBQBRQ1

3-line to 8-line decoders/demultiplexer

SN74HCS151-Q1

SN74HCS151QWBQBRQ1

8-to-1 multiplexer with Schmitt-trigger inputs

SN74HCS153-Q1

SN74HCS153QWBQBRQ1

Dual 4-to-1 multiplexer with Schmitt-trigger inputs

SN74HCS157-Q1

SN74HCS157QWBQBRQ1

Quadruple 2-to-1 multiplexer with Schmitt-trigger inputs

SN74HCS165-Q1

SN74HCS165QWBQBRQ1

8-bit PISO shift register

SN74HCS259-Q1

SN74HCS259QWBQBRQ1

Addressable latch

SN74HCS365-Q1

SN74HCS365QWBQBRQ1

Hex buffers and line drivers with 3-state outputs

SN74HCS367-Q1

SN74HCS367QWBQBRQ1

Hex buffer/line driver with non-inverting 3-state outputs

SN74HCS594-Q1

SN74HCS594QWBQBRQ1

8-bit SIPO shift register, push-pull output

SN74HCS595-Q1

SN74HCS595QWBQBRQ1

8-bit SIPO shift register, 3-state output

References and further information on new TI LOGIC packages

SN74HCS595-Q1 datasheet – TI

Optimizing Board Design for Supply Constrained Environments - (TI Applications)