This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer wants to drive the SPI signal between two separate boards. There are four twisted pairs between these two boards and the length is 1m. The twisted pair is from an Ethernet cable.
Is it possible? Do you have some suggestions on this?
B&R
Lijia
Hi Lijia,
Yes, I can make some suggestions.
I would recommend to use a source termination like this:
Rs is used to match the source (HCS244) to the transmission line (your twisted pair). Most twisted pair wires have impedance around 100 ohms, and the HCS device has an output impedance around 30 ohms, so I'd start with Rs = 75 ohms and see how that works. If they know the characteristic impedance of the twisted pair (transmission line), then they could match it more precisely based on the datasheet provided output impedances for the HCS device.
If you already have pairs, then it makes sense to use differential transceivers, e.g., SN65LVDT41/SN65LVDT14. This is very helpful if the environment can be noisy.