Hi sir/mam.,
I need to know the power consumption of the SN74LVCH16T245DGGR, SN74AVCH4T245PWR, SN74AVC4T774RSVR IC's. I have calculated the but I want to know whether calculation is correct or not. Kindly help me on this.
| VCCA | VCCB | ICCA | ICCB | F | Cpd | Cl | Nsw | U31 | SN74LVCH16T245DGGR | |
| 1.8 | 5 | 0.00002 | 0.00002 | 10000000 | 3E-12 | 1.5E-11 | 16 | Pstatic | 0.000036 | 0.0001 |
| 2.2E-11 | Ptra | 0.0015552 | 0.088 | |||||||
| Pdyn | 0.007776 | 0.06 | ||||||||
| 0.005204 | 0.02962 | |||||||||
| Power(mW) | 5.204 | 29.62 |
| VCCA | VCCB | ICCA | ICCB | F | Cpd | Cl | Nsw | SN74AVCH4T245PWR | ||
| 3.3 | 3.3 | 0.000008 | 0.000008 | 12000000 | 6E-11 | 1.5E-11 | 4 | Pstatic | 0.0000264 | 0.0000264 |
| 6E-11 | Ptra | 0.0313632 | 0.0313632 | |||||||
| Pdyn | 0.0078408 | 0.0078408 | ||||||||
| 0.011888 | 0.011888 | |||||||||
| In mW | 11.888 | 11.888 |
| VCCA | VCCB | ICCA | ICCB | F | Cpd | Cl | Nsw | SN74AVC4T774RSVR | ||
| 3.3 | 1.8 | 0.000008 | 0.000008 | 12000000 | 6E-11 | 1.5E-11 | 4 | Pstatic | 0.0000264 | 0.0000144 |
| 6E-11 | Ptra | 0.0313632 | 0.0093312 | |||||||
| Pdyn | 0.0078408 | 0.0023328 | ||||||||
| Cleff | 6E-11 | 0.011888 | 0.006488 | |||||||
| Power In mW | 11.888 | 6.488 | ||||||||
| Current in mA | 3.602424242 | 3.604444444 |