Part Number: TXS0102
Other Parts Discussed in Thread: TXU0102, TXU0202
Hi team,
My customer is consider to use TXS0102 for UART(4Mbps) (A-port 3.3V, B-port 5V).
But their concern is that they need to use ~2m cable between 2 boards.
They are currently testing it by using TXS EVM with soldering around 30cm cables in between two target boards and it work well,
but they are asking how to reduce the overshoot for the waveform.
Q1 : Does TXS0102 is right recommendation for them? (It is AVL device for them)
Q2 : Would you recommend the way how to reduce the overshoot in rising edge at TXS0102?

Best Wish,
Ernest Cho