This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUC16374: is it ok if input signal overshot to -0.8V?

Part Number: SN74AUC16374


Hi team,

Customer is usingSN74AUC16374 and input signal will be like yellow waveform as shown, it'll overshoot to -0.8V but our abs.max is -0.5V. Could you pls help to confirm if this overshoot will cause damage to the device?

Any reliability risk?

Thanks!

Rayna

  • Hi Rayna,

    I would first recommend to verify that this measurement is accurate -- it is very common to see excessive ringing when using a standard passive scope probe:

    The ground lead on the scope probe has a fairly significant length and loop area that contributes to ringing.

    It's best to either test with a differential probe or a very short ground lead.

    -

    If this is an actual undershoot and not just measurement error, then I would say that they should add some series resistance at the input to prevent excessive current.

    With -1V at the input, a resistor of value of only 10 ohms would be sufficient to limit current to 50 mA. I would recommend to use 100 ohms to keep any current through the diode low.